Linker for HC05 in CW v5.9

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Linker for HC05 in CW v5.9

877 次查看
timothymosher
Contributor I

I am trying to make binaries for some old code targeting an HC05.

 

The version of Freescale CodeWarrior that we are using (5.9.0.5292) does not appear to have an HC05 linker.

I can get the code to compile fine, but I cannot link.

 

Does anyone know what options are available to me here?

I would like to continue using CodeWarrior.

 

We have used this product to make binaries for our HC08 chips just fine.

标签 (1)
0 项奖励
回复
1 回复

695 次查看
trytohelp
NXP Employee
NXP Employee

Hi Timothy,

The HC05 is not supported by CodeWarrior for a long time.

The HC05, HC11, and HC16 have been approved for end of life the September 8, 2006.

I think the last version included HC05 was CW8/16V1.0 or CW MOT V1.0.

The versions of IDE used were 4.1.0629 or 4.2.0708.

These versions were released in 2000-2001.

Since September 2006 we don't have anymore CodeWarrior development tool supporting the HC05 devices.

I recommend you to check with Third Party:

    Cosmic Software - HC05 Products

    C6805 C Compiler for Freescale HC05 | Byte Craft Limited

    ...

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复