Linker error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linker error

9,547 Views
iam
Contributor I
Hi all !
 
I am getting an error when compiling a C application with references to an assembly function. Asm functions are defined in .s file and declared as extern in .c file. The linker error is undefined reference to ASM function.
 
Here are code:
jtag.s
Code:
; ================================================; Function : JTAG_Read_Bkru ; ================================================; input parameters; r0 : address of the register to read ; ================================================; output parameters; r1 : address to store the result  ; ================================================; r4 : used by TDO, TDI, TCK, TMS ; r5 : used by TDO, TDI, TCK, TMS; r6 : address bitmask ; r7 : output bitmask ; r8 : output value; r9 : scratch register; r10 : used to clear TDIJTAG_Read_Bkru INIT_JTAG MOV r6, #1  ; init address bitMask   MOV r7, #1  ; init output bitMask   MOV r8, #0 MOV r10, #0...

 
jtag.h
Code:
...extern void JTAG_Read_Bkru(unsigned char address, unsigned int *data);...

jtag.c
Code:
...unsigned int JTAG_Read_Debug_Status(){  unsigned int value;  //* Select ICEBreaker Scan Chain JTAG_Select_Scan_Chain(ICE_BREAKER);  //* Read the Debug Status register JTAG_Read_Bkru(ICE_DBG_STS, &value); return (value & ICE_DBG_STS_MASK);}...

It seems that .s file is not passed into linker. But .s file is in project.
Could you please help me with this problem ?
 
Thanks.
Labels (1)
0 Kudos
Reply
11 Replies

4,569 Views
CrasyCat
Specialist III

Hello

OK I took a look at the project you have attached.
Apparently you are targeting an ARM core. Am I right?

Build tools delivered with CodeWarrior for ARM are not supported and maintained by
Freescale.
You will have to request some help from ARM. They will be able to assist you in programming with their build tools.
Sorry for the confusion, I did not check first which CPU you were targeting.

CrasyCat

0 Kudos
Reply

4,569 Views
iam
Contributor I
Yes, you are right.
 
Thank you. Sorry for the lost time.
0 Kudos
Reply

4,569 Views
J2MEJediMaster
Specialist I
I'm looking at some HC12 assembly code here, and you need to use a XDEF declaration to make the function's name visible to other files. To wit:

XDEF JTAG_Read_Bkru

Your assembler may use the same declaration or something similar.

---Tom
0 Kudos
Reply

4,569 Views
CrasyCat
Specialist III

Hello

I am missing a little bit of context information here.

However, did you tell the label JTAG_Read_Bkru should be visible outside of the .s file?
Just add a

  xref JTAG_Read_Bkru


in your assembly source file.
 

CrasyCat

0 Kudos
Reply

4,569 Views
iam
Contributor I
Yes, JTAG_Read_Bkru should be visible outside the .s file.
 
The line you proposed to add is already exist in assembly file. But with some differences. 'EXTERN' is used instead of 'xref'. (i use Metrowerks CodeWarrior)
 
Thanks,
iam
0 Kudos
Reply

4,569 Views
J2MEJediMaster
Specialist I
OK, if EXTERN is being used in the assembly file for JTAG_Read_Bkru, that says the symbol and code are defined somewhere *other than this file*.

What you're wanting to do is *export* the symbol of the JTAG_Read_Bkru from this file, so that the function is visible to other the files. So you either need to use the 'XDEF' or 'XREF' (Crasycat's suggestion) declaration. Replace the EXTERN in the assembly file with either of these.

---Tom
0 Kudos
Reply

4,569 Views
iam
Contributor I
I have tried to use XDEF and XREF instead. The result was the same (
0 Kudos
Reply

4,569 Views
CrasyCat
Specialist III

Hello

Please send a whole project reproducing the trouble.

We will not be able to move forward without  a real project

CrasyCat

0 Kudos
Reply

4,569 Views
iam
Contributor I

Hello,

here is CW project reproducing error...

Thanks,

iam

0 Kudos
Reply

4,569 Views
J2MEJediMaster
Specialist I
OK... Is the assembler generating an object file?

---Tom
0 Kudos
Reply

4,569 Views
CrasyCat
Specialist III

Hello

Oups  I had a typo in my last message. In fact you HAVE to use XDEF not XREF in your assembly source file.

Sorry about the confusion.

I am not sure EXTERN is supported.

CrasyCat

0 Kudos
Reply