Linker Command File Syntax For CodeWarrior with the MPC5125

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linker Command File Syntax For CodeWarrior with the MPC5125

3,236 Views
Tim562
Senior Contributor I

Hi All, I find that I need to modify the CodeWarrior  Linker Command File for my MPC-5125 project and I'm having a difficult time finding documentation on this file and it's syntax. Can anybody point me to a download link for a manual or an appnote that covers this? I'm using Code Warrior for MobileGT ver 9.2, thanks!

~Tim

Labels (1)
0 Kudos
Reply
1 Reply

2,779 Views
Pavel
NXP Employee
NXP Employee

Look at attached file. This file is available in CodeWarrior MGT 9.2 folder.

Find the Chapter "Linker".


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply