Linker Command File Syntax For CodeWarrior with the MPC5125

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Linker Command File Syntax For CodeWarrior with the MPC5125

3,245 次查看
Tim562
Senior Contributor I

Hi All, I find that I need to modify the CodeWarrior  Linker Command File for my MPC-5125 project and I'm having a difficult time finding documentation on this file and it's syntax. Can anybody point me to a download link for a manual or an appnote that covers this? I'm using Code Warrior for MobileGT ver 9.2, thanks!

~Tim

标签 (1)
0 项奖励
回复
1 回复

2,788 次查看
Pavel
NXP Employee
NXP Employee

Look at attached file. This file is available in CodeWarrior MGT 9.2 folder.

Find the Chapter "Linker".


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复