Linker: Can't write application "boot_loader.elf".

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linker: Can't write application "boot_loader.elf".

Jump to solution
2,317 Views
DeveloperOne
Contributor I

Please help,

 

I have just installed "CodeWarrior for ColdFire V6.3" and when I hit F7 I get the following linker message:

 

Can't write application "boot_loader.elf".

An unknown error occurred when linking target "boot_loader" for project "mqx.mcp".

 

Any ideas? I am told that the project that I am trying to build can be built on other computers.

 

Thank you!

 

Labels (1)
0 Kudos
Reply
1 Solution
1,330 Views
J2MEJediMaster
Specialist I

What's the operating system version, and are you running 32-bit or 64-bit mode? Also, if everything else has been running smoothly, are you sure you have enough disk space left over, or are you trying to write to directory that you have no user rights to access?

 

---Tom

 

View solution in original post

0 Kudos
Reply
4 Replies
1,331 Views
J2MEJediMaster
Specialist I

What's the operating system version, and are you running 32-bit or 64-bit mode? Also, if everything else has been running smoothly, are you sure you have enough disk space left over, or are you trying to write to directory that you have no user rights to access?

 

---Tom

 

0 Kudos
Reply
1,330 Views
DeveloperOne
Contributor I

Master,

 

Thank you for your reply and I apologize if I wasted any of your time. It seems that the project that I was given, in fact, did not build on other build machines. I can successfully compile and link now.

 

Thank you!

Big D

0 Kudos
Reply
1,330 Views
J2MEJediMaster
Specialist I

It is my job to help solve problems, so no time was wasted. By the way, what was causing the build problem?

 

---Tom

0 Kudos
Reply
1,330 Views
DeveloperOne
Contributor I

Well, that was an older project that I was testing, so I moved to the latest project and it worked fine. So, I didn't spend any more time on trying to resolve the old projects issue.

Thanks~

0 Kudos
Reply