Length of variable names? CW 5.7.0.2015...MC9S08RE16

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Length of variable names? CW 5.7.0.2015...MC9S08RE16

1,532 Views
stevec
Contributor III
    What is the maximum length of varaible names in Code Warrior? I cant seem to find it anywere.

Steve
Labels (1)
0 Kudos
Reply
1 Reply

515 Views
CrasyCat
Specialist III
Hello
 
You are using CodeWarrior for HC08. Right?
 
Look at {Install}\Help\PDF\Compiler_HC08.pdf.
Chapter "ANSI-C Front End", section "Implementation Features" -> Translation Limitations"  describes all the internal limitation of the compiler.
 
In table 8.4 I could find
"Number of initial characters in an internal identifier or macro name 32,767".
 
 
CrasyCat
0 Kudos
Reply