JTAG schematics

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JTAG schematics

8,438件の閲覧回数
JTAGSchematics
Contributor I
Hi,
 
I'd like to know if it's possible to someone inform me where can I get schematics for JTAG interface.
 
I've got to program a 56F8013, could someone help me with some schematic? 
 
Are those schematics, found on Evaluation Board manuals, valid? (Those that use some buffers and are pluged in the parallel port)
 
 
Thanks in advance,
 
 
Northon
ラベル(1)
タグ(1)
0 件の賞賛
返信
5 返答(返信)

3,065件の閲覧回数
Fabian
Contributor I
HI, I am new in the DSP's world, and I bought a DSP724 and I need to now which and where can I get the programmer for it?? please help me thanks
0 件の賞賛
返信

3,065件の閲覧回数
JTAGSchematics
Contributor I
I adapted this attached schematic for a simple 56F8013 and it ran out.


It works fine.


Bye
0 件の賞賛
返信

3,065件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
I checked with my colleague working on the hardware team.
You can use the schematic from EVMs manual (8367EVM for example).
Also the parralel jtag converter is described in flash_over_jatg_v2 manual (faq-19720)
Hope this will help you
 
Regards
Pascal
0 件の賞賛
返信

3,065件の閲覧回数
JTAGSchematics
Contributor I
Hi,
 
I'd like first to thank Pascal for the help he provided, I'm studying the schameatics he suggested and it's the one i needed. The thing is that, while I was analyzing it I've found some things there that i coudn't understand. There are two CIs (74HC244DW and 74LCX244DW) that have their pins 7, respectivally, connected to a box with a number 1 wrote in it. I just can't understand what that means.
 
If anyone please have sometime to check it out and help me, I'd be thankful.
 
Regards
 
0 件の賞賛
返信

3,065件の閲覧回数
bobc
Contributor II
I think the square with a 1 in just represents a Test Point or pad.
0 件の賞賛
返信