JTAG schematics

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JTAG schematics

8,452 Views
JTAGSchematics
Contributor I
Hi,
 
I'd like to know if it's possible to someone inform me where can I get schematics for JTAG interface.
 
I've got to program a 56F8013, could someone help me with some schematic? 
 
Are those schematics, found on Evaluation Board manuals, valid? (Those that use some buffers and are pluged in the parallel port)
 
 
Thanks in advance,
 
 
Northon
Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

3,079 Views
Fabian
Contributor I
HI, I am new in the DSP's world, and I bought a DSP724 and I need to now which and where can I get the programmer for it?? please help me thanks
0 Kudos
Reply

3,079 Views
JTAGSchematics
Contributor I
I adapted this attached schematic for a simple 56F8013 and it ran out.


It works fine.


Bye
0 Kudos
Reply

3,079 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
I checked with my colleague working on the hardware team.
You can use the schematic from EVMs manual (8367EVM for example).
Also the parralel jtag converter is described in flash_over_jatg_v2 manual (faq-19720)
Hope this will help you
 
Regards
Pascal
0 Kudos
Reply

3,079 Views
JTAGSchematics
Contributor I
Hi,
 
I'd like first to thank Pascal for the help he provided, I'm studying the schameatics he suggested and it's the one i needed. The thing is that, while I was analyzing it I've found some things there that i coudn't understand. There are two CIs (74HC244DW and 74LCX244DW) that have their pins 7, respectivally, connected to a box with a number 1 wrote in it. I just can't understand what that means.
 
If anyone please have sometime to check it out and help me, I'd be thankful.
 
Regards
 
0 Kudos
Reply

3,079 Views
bobc
Contributor II
I think the square with a 1 in just represents a Test Point or pad.
0 Kudos
Reply