Is the CodeWarrior USB Tap useful in a Linux environment?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is the CodeWarrior USB Tap useful in a Linux environment?

2,124 次查看
emagii
Contributor II

We have boards using the MPXS2010 PowerPC processor.
We have an environment where we develop code using GCC under Cygwin.
We are moving away from Cygwin to run a Linux virtual machine, with GCC running with 'wine'.

Next step is to have a native PowerPC compiler under Linux.

I understand that CodeWarrior does not allow compiling natively on Linux (wine is not an alternative)

I need to understand how I can debug the code.

We have a Trace-32 that is used to debug code, but we need an additional seat, and the Trace-32 is very expensive. I happen to have a "CodeWarrior USB TAP, rev F"

This is no longer sold.

  • What is the latest version of CodeWarrior, where this is supported on Windows?
  • Can the "CodeWarrior USB TAP," be used by any other toolchain?
  • Can the "CodeWarrior TAP" (with Ethernet) which is still active be used by anything but CodeWarrior?
0 项奖励
回复
2 回复数

2,016 次查看
emagii
Contributor II

It appears that is it supported in the CodeWarrior 11 running under Windows.

0 项奖励
回复

2,107 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I'm afraid that CodeWarrior (USB) TAP is not an option.

MPXS2010 was an 'industrial' version of MPC5643L microcontroller and these devices are not supported by this tool.

Regards,

Lukas

0 项奖励
回复