Internal Linker Error: File: ELF_gen.c ???

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Internal Linker Error: File: ELF_gen.c ???

2,935 Views
Karl_H
Contributor III

CW version = 5.9.0

Processor = PowerPC 8270

 

What is the meaning of

 

Internal Linker Error: File: 'ELF_gen.c' line 978

 

There is no such file in my code or the code delivered with CodeWarrior. And searching the help files on this turns up nothing.

 

I am trying to configure a bare-bones application. I used the same procedure for this application as for another one I recently created that builds without this error.

 

KH

Labels (1)
0 Kudos
Reply
3 Replies

1,991 Views
J2MEJediMaster
Specialist I
Internal errors are usually a bad sign. Please file a service request on this. Be prepared to supply a project and source that does not give away your IP but can reproduce the problem. Click here to submit a service request.
0 Kudos
Reply

1,991 Views
Karl_H
Contributor III

It turns out that I had conflicting addresses for the entry point in the configuration. When I fixed that, the problem went away.

 

KH

 

0 Kudos
Reply

1,991 Views
CompilerGuru
NXP Employee
NXP Employee

Would still be good to get it fixed for other users so the error could be improved from

"internal linker error" to "conflicting entry point address" :smileyhappy:

 

So please file a report...

 

Daniel

 

0 Kudos
Reply