Installation on Windows 11

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installation on Windows 11

3,119件の閲覧回数
jdub8595
Contributor I

I am able to install CodeWarrior for HCS12(X) Microcontrollers v5.2 on a machine with Windows 11. However, the core DLL cannot be registered. I have tried the suggested regserver batch file as an Administrator and manually using regsvr32. No luck running the IDE. 

Any one have any luck with using CodeWarrior for HCS12(X) Microcontrollers v5.2 on Windows 11?

タグ(1)
0 件の賞賛
返信
2 返答(返信)

3,080件の閲覧回数
Alphabert_Liu
NXP Employee
NXP Employee

Hello @jdub8595 

I've already installed the CodeWarrior for HCS12(X) Microcontrollers v5.2 on my computer with Win 11 without any question, and I run the IDE sucessfully. Could you please give me a more detailed description so that I could find the point that is confusing you.

BR

Liu

0 件の賞賛
返信

2,852件の閲覧回数
e_taylor
Contributor III
Hi Alphabert_Liu, I have never had any luck getting the IDE to run under Win 10. Did you use compatibility mode? I had issues with breakpoints not working.
0 件の賞賛
返信