Install codewarrior for microcontrollers V62 In vista 64 bits

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Install codewarrior for microcontrollers V62 In vista 64 bits

跳至解决方案
4,005 次查看
JuanManuel
Contributor I

Hello every body

 

nice to met us

 

Some one can help me i cant install codewarrior for microcontrollers V62 In Windows vista 64 bits the installer has no errors but cant complete the installer

标签 (1)
0 项奖励
回复
1 解答
1,946 次查看
J2MEJediMaster
Specialist I

I am sorry, but that version of CodeWarrior software only works with 32-bit Microsoft Vista.

 

---Tom

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,946 次查看
nonarKitten
Contributor II

I installed the application under Vista 32-bit on a separate partition, then in x64 Windows-7, ran D:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.2\bin\regservers.bat first and the program has worked just fine. I haven't tried copying the folder across and am still running from the D drive. This shows that the problem is primarily with the installer and not CodeWarrior!

0 项奖励
回复
1,947 次查看
J2MEJediMaster
Specialist I

I am sorry, but that version of CodeWarrior software only works with 32-bit Microsoft Vista.

 

---Tom

 

0 项奖励
回复
1,946 次查看
JuanManuel
Contributor I

Thanks Tom, so what can i do, i dont have other computer and the OS is original. there is no way to install the program?

0 项奖励
回复