Install codewarrior for microcontrollers V62 In vista 64 bits

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Install codewarrior for microcontrollers V62 In vista 64 bits

ソリューションへジャンプ
3,999件の閲覧回数
JuanManuel
Contributor I

Hello every body

 

nice to met us

 

Some one can help me i cant install codewarrior for microcontrollers V62 In Windows vista 64 bits the installer has no errors but cant complete the installer

ラベル(1)
0 件の賞賛
返信
1 解決策
1,940件の閲覧回数
J2MEJediMaster
Specialist I

I am sorry, but that version of CodeWarrior software only works with 32-bit Microsoft Vista.

 

---Tom

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,940件の閲覧回数
nonarKitten
Contributor II

I installed the application under Vista 32-bit on a separate partition, then in x64 Windows-7, ran D:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.2\bin\regservers.bat first and the program has worked just fine. I haven't tried copying the folder across and am still running from the D drive. This shows that the problem is primarily with the installer and not CodeWarrior!

0 件の賞賛
返信
1,941件の閲覧回数
J2MEJediMaster
Specialist I

I am sorry, but that version of CodeWarrior software only works with 32-bit Microsoft Vista.

 

---Tom

 

0 件の賞賛
返信
1,940件の閲覧回数
JuanManuel
Contributor I

Thanks Tom, so what can i do, i dont have other computer and the OS is original. there is no way to install the program?

0 件の賞賛
返信