Importing/Moving CodeWarrior 10.0  (Build: 100611) ProcessorExpert.pe file for HC08 processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Importing/Moving CodeWarrior 10.0  (Build: 100611) ProcessorExpert.pe file for HC08 processor

1,562 次查看
jjordan
Contributor I

I am trying to import a CodeWarrior 10.0 (Build: 100611) project but the ProcessorExpert.pe does not show any of the components in the directory structure.

 

In the project's other workspace, there was the ProcessorExpert.pe file and it had 3 folders below it. Within these folders there were the processor and several components. When I import, it only shows the xml file itself (ProcessorExpert.pe) with an icon with blue "<>" symbols on it. 

The components still show up in the original project.

 

 When I import I do "File -> Import -> General -> Existing Projects into Workspace" and I select the directory with the .cproject file.

Am I importing the project correctly or do I need to pass the workspace directory around as well?

 

Thank you,

Josh

标签 (1)
0 项奖励
回复
1 回复

1,085 次查看
jjordan
Contributor I

Nevermind.

If you select "Processor Expert -> Bring Processor Expert Views"  they will show up.

0 项奖励
回复