I'm trying to create a Processor Expert project for S12VR48 using a new install of CW v5.2 for HCS12.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I'm trying to create a Processor Expert project for S12VR48 using a new install of CW v5.2 for HCS12.

ソリューションへジャンプ
1,693件の閲覧回数
michaelgoudey
NXP Employee
NXP Employee

This version of CodeWarrior includes Processor Expert v3.06 for HCS12(x).  First, I create a basic project and then try to open Processor Expert view.  There is a message stating selected CPU 'MC129S12VR48' is not supported by Processor Expert.  The dialog asks me if I want to select a different CPU.

 

I look under the installation directory <CWS12v5.2>/Processor Expert/CPUs.  Sure enough there is a directory there "MC9S12VR64_48".  However, the components library view only shows VR16 and VR32.  Can someone explain why VR48 and VR64 are not available?

 

Thanks, Michael Goudey

ラベル(1)
0 件の賞賛
返信
1 解決策
1,495件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Michael,

The VR48 is fully supported on HC12 v5.1.

Under V5.2, according to the release note, Processor Expert (PEx) should support the device too.

It's not the case.

VR48 and VR64 is not supported by PEx.

At this time I can not provide you workaround excepted recommend you to use V5.1 and not V5.2.

I will check with Product Manager.

Keep you informed.


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,496件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Michael,

The VR48 is fully supported on HC12 v5.1.

Under V5.2, according to the release note, Processor Expert (PEx) should support the device too.

It's not the case.

VR48 and VR64 is not supported by PEx.

At this time I can not provide you workaround excepted recommend you to use V5.1 and not V5.2.

I will check with Product Manager.

Keep you informed.


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,495件の閲覧回数
michaelgoudey
NXP Employee
NXP Employee

Thank you Pascal.  I hope we can get this fixed, as I am surprised the newer CodeWarrior software does not enable everything from the previous version.

0 件の賞賛
返信
1,495件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Michael,

Just to inform you I've contacted Processor Expert team (PEx).

All VR devices should be supported through PEx in the V5.2.

The team logged it in the bug base and it should be fixed asap.

At this time I can not give you more information.

Regarding the devices supported on V5.2 vs V5.1.

The V5.2 is supporting the last devices only which are:

(2) This release includes support for the following derivatives:

    - MC9S12C128, MC9S12C32, MC9S12C64, MC9S12C96

    - MC9S12G128, MC9S12G96

    - MC9S12GC128, MC9S12GC16, MC9S12GC32, MC9S12GC64

    - MC9S12GN16, MC9S12GN32

    - MC9S12P32, MC9S12P64, MC9S12P96, MC9S12P128

    - MC9S12XEP100, MC9S12XEP768

    - MC9S12XEQ384, MC9S12XEQ512

    - MC9S12XET256

    - MC9S12XS128, MC9S12XS256, MC9S12XS64

    - MC9S12VR16, MC9S12VR32, MC9S12VR48, MC9S12VR64

If you are using another device you need to install and use the V5.1.

Regards

Pascal

0 件の賞賛
返信