How to See the Registors when a programme is debugging..

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to See the Registors when a programme is debugging..

2,369件の閲覧回数
Ranjicgnr
Contributor I
I am trying to use PWM in 56F8013 for my project. I am using Code Warrior 7.2 hybrid release. In that i cant see the pheripheral registers when i am running the project. It is showing only cpu registers. How can i see the pheripheral registers in the debugging mode. This pheripheral registers are avilable when i an runnung an example programme that already there in the code warrior. But it is not commin when i am creating a project. I am using the processor expert also in my programm. Please help me.
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,148件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
According to the info you provided it seems you're using an old version.
Freescale 56800/E Digital Signal Controllers Version 8.2
You can download this version on our web site via the link:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CWS-568-CX#
The Special edition license is installed by default.
If you need another version of the license please contact your local distributor.
You can have several versions installed on the same PC.
There is only one restriction: install them on separate folder.
If you're using an old version, please backup your project before to try it with this new version.
If you will meet some compatibility issue you could back to the older version without problem.
Regarding your question.
After to launch the debug session and can acces to the register using the menu View ¦ register or View ¦ Register Details.
 
Regards
Pascal
 
0 件の賞賛
返信