Help with finding the right codewarrior!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help with finding the right codewarrior!

2,696件の閲覧回数
mitchkk
Contributor I

Hello, I am looking all over the web to try and find the codewarrior program i use in my school for c++. I see that this is the only website and when i go to the download sections, there are so many to choose from! i need to find out which one is the right one to pick & were i can get the codewarrior IDE for wndows 7, 64 bit computer! any help would be great!

cout<<"help with codewarrior"<<endl;

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,312件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Kelman,

Here is a tool that may help you get the best option for you. CodeWarrior Selector Tool​

Regards,

0 件の賞賛
返信

2,312件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

What is the part number of the MCU or Processor that you are using?

0 件の賞賛
返信

2,312件の閲覧回数
derek_lau
Contributor III
0 件の賞賛
返信

2,312件の閲覧回数
J2MEJediMaster
Specialist I

It depends upon what you are trying to do here. If your intent is to write and run C++ programs on your desktop/laptop, CodeWarrior does not do that. (It used to be able to generate Windows apps, but that capability has been discontinued years ago.)

 

If you are going to be writing programs for embedded processors, you need to tell us which processor you are targeting before we can give you an answer. As you have noticed, there are many different versions of CodeWarrior, each which generates code for a specific processor.

 

---Tom

0 件の賞賛
返信