Help with finding the right codewarrior!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help with finding the right codewarrior!

2,734 Views
mitchkk
Contributor I

Hello, I am looking all over the web to try and find the codewarrior program i use in my school for c++. I see that this is the only website and when i go to the download sections, there are so many to choose from! i need to find out which one is the right one to pick & were i can get the codewarrior IDE for wndows 7, 64 bit computer! any help would be great!

cout<<"help with codewarrior"<<endl;

Labels (1)
0 Kudos
Reply
4 Replies

2,350 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Kelman,

Here is a tool that may help you get the best option for you. CodeWarrior Selector Tool​

Regards,

0 Kudos
Reply

2,350 Views
TICS_Fiona
NXP Employee
NXP Employee

What is the part number of the MCU or Processor that you are using?

0 Kudos
Reply

2,350 Views
derek_lau
Contributor III
0 Kudos
Reply

2,350 Views
J2MEJediMaster
Specialist I

It depends upon what you are trying to do here. If your intent is to write and run C++ programs on your desktop/laptop, CodeWarrior does not do that. (It used to be able to generate Windows apps, but that capability has been discontinued years ago.)

 

If you are going to be writing programs for embedded processors, you need to tell us which processor you are targeting before we can give you an answer. As you have noticed, there are many different versions of CodeWarrior, each which generates code for a specific processor.

 

---Tom

0 Kudos
Reply