Help me !!!!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help me !!!!

2,532件の閲覧回数
campcerkit
Contributor I
I use 56f8013 for my project . I new for Freescale
I try to use Processor Expert
1. I use PWM from Bean Selector 
      set       Period   2ms
      set      Starting pulse width  1mS
      i measue output . Yes it work
2. I use PWMMC from Bean Selector
  Why not output signal from output pin ??
  
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,131件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hello,
 
there are some examples delivered on the Installation.
For the Demoboard 56F8013 there is a example project using PWM.
Please have a look to the folder:
 \Stationery\Processor_Expert_Examples\DemoApplications\56F8013_DemoBoard\PWM_Example
 
hope this will help you.
 
regards
Pascal
0 件の賞賛
返信

1,131件の閲覧回数
ProcessorExpert
Senior Contributor III
We need more detailed information in order to evaluate the problem. Could you please provide us a project demonstrating this problem?

best regards
Vojtech Filip
Processor Expert Support Team
UNIS
0 件の賞賛
返信