Getting FlexLm to recognize the USB Dongle

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting FlexLm to recognize the USB Dongle

4,318 Views
v_dave
Contributor IV
Hello All,
 
I have downloaded MW_FLEXlm_V1_4.exe from freescale.com and ran the installation.  After I install FlexLm I plug n the USB Dongle and I am prompted to install the drivers.  I select automaticlly find the correct drivers and the Wizard comes bck with unable to find the drivers.
 
The little 1 sheet of instructions that came with the dongle tell me that when FlexLM install starts to make sure I select install Dongle Drivers.  I never see this option during installation.
 
Is there a different version of the FlexLm I need to install?
 
Thanks,
Dave
Labels (1)
0 Kudos
Reply
2 Replies

1,311 Views
CrasyCat
Specialist III
Hello
 
As far as I can tell, you need to install "Standard Driver Installer"  from following URL:
 
Then check whether your dangle is recognized
If dangle is not recognized, please install "Driver Update" as well.
 
CrasyCat
0 Kudos
Reply

1,311 Views
v_dave
Contributor IV
Thanks. 
 
The Driver update fixed the problem.
 
Dave
0 Kudos
Reply