Freescale Code Warrior IDE version 5.7.0 Crashes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freescale Code Warrior IDE version 5.7.0 Crashes

3,801件の閲覧回数
BoSCHoW
Contributor II
Hello all,

If i click directly on the project CodeWarrior opens it and i can make changes and compile my code, but when I try to add new file it just crushes without any warrnings. The same thing happen if I rush CodeWarrior through a short cut, and then i try to open a project. Is there any updates for this "bug"?

Thanks and
Best Regards,
BoSCHoW.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,568件の閲覧回数
BoSCHoW
Contributor II
Hi,

the uninstalation of groove removed this "microsoft bug". Thanks for the info.
P.S. Shouldnt microsoft test their application more seriously?

Best Regards,
BoSCHoW.
0 件の賞賛
返信

1,568件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
As guess check this thread,
http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&message.id=1143
there is a bug with MS-Groove, it does not only affect CW tough.
That thread also shows the work around.

Daniel
0 件の賞賛
返信