Finding the version of codewarrior?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Finding the version of codewarrior?

3,551件の閲覧回数
Ratzlaff
Contributor I
I'm in the process of filling out the license transfer form and I dont know what version of codewarrior I have. (the example is: Code warrior for HCS08, standard edition v5.0)

err, I see nothing like that on my box, or in the about menu of the program. What it does say is: CodeWarrior IDE version 5.5.1.1409. I assume its a pre-freescale release? Is that enough, or should it be CodeWarrior for x86 v5.5?
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,879件の閲覧回数
J2MEJediMaster
Specialist I
You're getting these numbers when you select Help | About Freescale CodeWarrior, right? See if the About window has an Installed Products button and click on that for a detailed version number. It sounds perhaps like you're already doing that. So, yes, just enter the information as displayed.

---Tom
0 件の賞賛
返信

1,879件の閲覧回数
Ratzlaff
Contributor I
Yeah, in the installed products it is: CodeWarrior Development Studio for Windows, Version 9.2

Thanks!
0 件の賞賛
返信