Failed to write in RAM..

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Failed to write in RAM..

1,056件の閲覧回数
hrishikesh23
Fresh Out Contributor

Dear All,

 

                 Can anybody guess what could be the Issue ..under hardware daignostic ..when i carrry out test for reading it continouslyy reads the same value but hte value i write keep on changing..anybody can guess whats going wrong.

 

All configuration files are correct checked with freescale People.

 

Read  0x00 at address: 0x00100000
Timestamp:  Tue Dec 20 16:42:22 2011
:  --------------------

 ============================================

  Wrote  0x67 at address: 0x00100000
Timestamp:  Tue Dec 20 16:42:29 2011
:  --------------------

 ============================================

  Read  0x00 at address: 0x00100000
Timestamp:  Tue Dec 20 16:42:57 2011
:  --------------------

 ============================================

  Read  0x00 at address: 0x00100000
Timestamp:  Tue Dec 20 16:42:59 2011
:  --------------------

ラベル(1)
0 件の賞賛
返信
1 返信

940件の閲覧回数
hrishikesh23
Fresh Out Contributor

Dear All,

 

               Please go through the Attached File.

0 件の賞賛
返信