Export CodeWarrior V5.0 projects to V10.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Export CodeWarrior V5.0 projects to V10.0

1,184 次查看
Coyote
Contributor I

Hello,

I installed the CodeWarrior V10 in Windows7 64bits.

It is possible Export my current projects CodeWarrior V5.0(Windoows XP)  to CodeWarrior V10.0(Windows7 64bits) ?

 

Thank you

标签 (1)
0 项奖励
回复
1 回复

832 次查看
NavidadRedivivu
Contributor III

I am assumming that you are targetting S08/RS08 or ColdFire. You can import "old" MCP projects in MCU 10. This feature is documented here (there may be also an application note on this). You should use this tool with caution though. You will most probably need to do some manual work too, but this pretty much depends on the complexity of your project(s).

0 项奖励
回复