Export CodeWarrior V5.0 projects to V10.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Export CodeWarrior V5.0 projects to V10.0

1,168 Views
Coyote
Contributor I

Hello,

I installed the CodeWarrior V10 in Windows7 64bits.

It is possible Export my current projects CodeWarrior V5.0(Windoows XP)  to CodeWarrior V10.0(Windows7 64bits) ?

 

Thank you

Labels (1)
0 Kudos
Reply
1 Reply

816 Views
NavidadRedivivu
Contributor III

I am assumming that you are targetting S08/RS08 or ColdFire. You can import "old" MCP projects in MCU 10. This feature is documented here (there may be also an application note on this). You should use this tool with caution though. You will most probably need to do some manual work too, but this pretty much depends on the complexity of your project(s).

0 Kudos
Reply