Error message when generating S-records for MC56F8345 with CW 56800/E v7.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error message when generating S-records for MC56F8345 with CW 56800/E v7.3

1,905 Views
running_warrior
Contributor I
I built a fw project for mc56f8345 with codewarrior for 56800/E v7.3 and tried to download generated S-Record file into dsp's flash memory with parallel flash programmer, this error message popped our saying:
 
"CHawkV2::VirtualImage::LoadFile: S-Record data must be given in whole WORDS"
 
I am sure I selected the combined .elf.s file instead of .elf.p.s or .elf.x.s. Another fact may be interseting: I can successfully download the generated .elf file. Do you have any suggestion what may cause this issue?
 
Thanks,
 



J2MEjediMaster added more precise header with MCU type and CW version

Message Edited by J2MEJediMaster on 2007-04-24 10:44 AM

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

740 Views
trytohelp
NXP Employee
NXP Employee
I never heard similar problem with the DSP 7.3.
Can I suggest you to try with the DSC 8.0 ?
You can download this version on our web site via the link:

The Special edition license is installed by default.
If you need another version of the license please contact your local distributor.
You can have several versions installed on the same PC.
There is only one restriction: install them on separate folder.

The DSC 8.1is a patch for the DSC8.0 (must be installed in first)
You can download this version on our web site via the link:
http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600617882140B

Hope this will help you.
Else please contact the support team.

- Go to following URL: http://www.freescale.com/TechSupport
- Click on Submit a Service Request. You will come to a login page.
- You can submit your request through the web from there.

Pascal

0 Kudos
Reply