ELF is not in expected HALT mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ELF is not in expected HALT mode

5,867 次查看
sai
Contributor I
When I try to step into next instruction or  somtimes put a break point or do a hard reset from the CodeWarrior IDE I get a message that says:

ELF is not in expected HALT mode or
ELF is not in expected STOP mode

Any idea what this means. Thanks for any inputs.

I'm using USB TAP to connect to target, with a default clock speed of 4.03 MHz. CodeWarrior version 8.7.

-Sai



Message Edited by sai on 2007-08-27 08:13 PM

Message Edited by sai on 2007-08-27 08:15 PM
标签 (1)
0 项奖励
回复
4 回复数

1,417 次查看
scancath
Contributor I
Hi,
 
I'm trying to connect USB TAP to our custom board. I'm getting the following messages
" Failed to freeze at negation of hreset" and "ELF is not in expected HALT mode" messages.

I presume some thing fundamental is wrong with this board. Any pointers on when I would see this type of messages?

Thanks  a bunch,
Prasad 
0 项奖励
回复

1,417 次查看
CrasyCat
Specialist III
Hello
 
I would recommend you to create a new post for that issue.
 
Make sure you specify which target and version of CodeWarrior you are using.
To retrieve that info:
- Start CodeWarrior
- Select Help -> About Freescale CodeWarrior
- Click on "Install Products"
- CodeWarrior version used is displayed on top in the Installed Products dialog.
 
CrasyCat
0 项奖励
回复

1,417 次查看
trytohelp
NXP Employee
NXP Employee
Hi,
 
Can you please give us the tool version used ?
To do that you must:
* CW:
Start the IDE and click on Help | About Metrowerks CodeWarrior.
Click on Installed Products 
Provide us all info displayed.
Or you can save them in a txt file.
Pascal
0 项奖励
回复

1,417 次查看
sai
Contributor I
Another freescaler has posted a reply to this question in CodeWarrior for ColdFire and Power forum.

Thanks anyway.
-Sai
0 项奖励
回复