Does CodeWarrior support batch build multiple projects with .mcp file given?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does CodeWarrior support batch build multiple projects with .mcp file given?

4,730 次查看
trotin
NXP Employee
NXP Employee
CPU: ColdFire
CodeWarrior: V6.1
 
We usually use IDE mode to develop our projects.
But in later phase, we may have to rebuild all of the projects at a time.
So I wonder  if there is some way to enable batch run.
 
The procedure is expected to be:
1) open projectA.mcp
2) build
3) close projectA.mcp
4) open projectB.mcp
5) build
6) close projectB.mcp
...
 
 
标签 (1)
0 项奖励
回复
4 回复数

2,092 次查看
CompilerGuru
NXP Employee
NXP Employee
Check the cmdide.exe in the bin folder, use

CmdIDE.exe /?


to see the available options.

Daniel
0 项奖励
回复

2,092 次查看
trotin
NXP Employee
NXP Employee
It works perfect for dozens of projects, so many thanks~~
0 项奖励
回复

2,092 次查看
CrasyCat
Specialist III
Hello
 
There are different ways of automating build process for multiple projects.
 
You can use Microsoft COM automation from a Perl or Visual Basic Script. Please refer to {Install}\Help\PDF\IDE_5.7_Automation_Guide.pdf Chapter "Microsoft COM Automation" for more information on that.
 
You can use use a TCL script instead to do that.Please refer to {Install}\Help\PDF\IDE_5.7_Automation_Guide.pdf Chapter "Command Window Scripting" for more information on that.
 
CrasyCat
0 项奖励
回复

2,092 次查看
trotin
NXP Employee
NXP Employee
Thanks, I believe those to be effective!
However, I think "cmdide.exe" is more directive and easy-understanding.  :smileyhappy:
 
------------
 
Hello
 
There are different ways of automating build process for multiple projects.
 
You can use Microsoft COM automation from a Perl or Visual Basic Script. Please refer to {Install}\Help\PDF\IDE_5.7_Automation_Guide.pdf Chapter "Microsoft COM Automation" for more information on that.
 
You can use use a TCL script instead to do that.Please refer to {Install}\Help\PDF\IDE_5.7_Automation_Guide.pdf Chapter "Command Window Scripting" for more information on that.
 
CrasyCat


Message Edited by trotin on 2008-10-06 02:23 AM
0 项奖励
回复