Debugging two projects

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debugging two projects

1,280 次查看
Eric_t
Contributor III

Hi everybody,

 

Currently I use CW5.1 and mc9s12xdt512 controller.

 

I have two separate projects, one is the bootloader and the other is the firmware application.

I have merge the bootloader to application project using the HEXFILE and everything works as it is expected.

Since I merge the bootloader with HEXFILE, I can debug only the application project and not bootloader.

Is there a way to be able to debug the two project at the same time?

 

I have already done this with kinetis and KDS IDE.

As far as I can remember, the KDS only needs to have at the workspace the two projects and the eclipse debugger automatically switches between two projects.   

 

Thank you.

标签 (1)
0 项奖励
回复
1 回复

1,032 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello

Does this can help you ?

How to support multiple targets in CodeWarrior(Classic, Eclipse)/KDS  


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复