Debugging from two computer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging from two computer

1,439件の閲覧回数
Teckna
Contributor V

Hi everyone,

 

I have two computer where I installed CW 10. The first is an XP computer (32 bit) where the installation path is "c:\program files\freescale\cw mcu v10.1"; the second one is a 7 computer (64 bit) where the installation path is "c:\program files (x86)\freescale\cw mcu v10.1". I have a NAS containing the workspace, the project and all the source files.

I can successfully open and build the project from both the computers. If I build the project on the XP computer, then I can even debug it on the same computer. However if I try to debug the project from the 7 computer I get the error

 

"make: *** No rule to make target `C:\Program Files\Freescale\CW MCU v10.1\MCU\ARM_EABI_Support\ewl\EWL_C\include\lib_ewl.prefix', needed by `Sources/main.obj'."

 

On the contrary, if I build the project on the 7 computer, then I can even debug it on the same computer. However if I try to debug the project from the XP computer I get the error

 

"make: *** No rule to make target `C:\Program Files (x86)\Freescale\CW MCU v10.1\MCU\ARM_EABI_Support\ewl\EWL_C\include\lib_ewl.prefix', needed by `Sources/main.obj'."

 

I made some investigation and I found that the file .\sources\main.d, generated by the building process related to the XP computer, contains the dependency list of the source file, that is written in a resolved form:

 

...

C:\Program Files\Freescale\CW\ MCU\ v10.1\MCU\ARM_EABI_Support\ewl\EWL_C\include\lib_ewl.prefix \

C:\Program Files\Freescale\CW\ MCU\ v10.1\MCU\ARM_EABI_Support\ewl\EWL_C\include\common.prefix \

C:\Program Files\Freescale\CW\ MCU\ v10.1\MCU\ARM_EABI_Support\ewl\EWL_C\include\ewl_c_version.h \

...

 

(A similar file is generated by the building process on the 7 computer where "Program Files" is substituted from "Program Files (x86)")

 

Is there a way to output this file in a non resolved form such:

 

...

${CW_INSTALLATION_PATH}\MCU\ARM_EABI_Support\ewl\EWL_C\include\lib_ewl.prefix \

${CW_INSTALLATION_PATH}\MCU\ARM_EABI_Support\ewl\EWL_C\include\common.prefix \

${CW_INSTALLATION_PATH}\MCU\ARM_EABI_Support\ewl\EWL_C\include\ewl_c_version.h \

...

 

where CW_INSTALLATION_PATH can be a system environment variable representing the installation path of CW?

Or is there another method to debug the same network project from different computers (maybe even at the same time)?

 

I would like to avoid uninstalling CW from one computer and then reinstalling it in the same path as the other computer.

 

Many thanks

Teckna

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,068件の閲覧回数
Teckna
Contributor V

No one can help?

0 件の賞賛
返信

1,068件の閲覧回数
J2MEJediMaster
Specialist I

You probably need to file a service request on this. Click here to do that.

 

---Tom

0 件の賞賛
返信