Debugger lost communication with target

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugger lost communication with target

1,784件の閲覧回数
Dekabrist
Contributor I

I debug my project. When I stop execute programm ("Debug/Break" or Breakpoint) Debuger stop correctly, but during time (about 3-5 minuts) lost communication with board and output error message (see attachment) even if I not activate debug functions in this time.

What idea about this trouble?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

954件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

 

This is not easy to determine the cause of the problem.
The better way will be to log it directly in the Technical support system.
Please use Freescale on line support web page.
  - Go to following URL: http://www.freescale.com/TechSupport
  - Click on Submit a Service Request. You will come to a login page.
  - You can submit your request through the web from there.

Please provide us more details about the Tool version used.
To do that you must:
* CW:
Start the IDE and click on Help | About Metrowerks CodeWarrior.
Click on Installed Products 
Provide us all info displayed.
Or you can save them in a txt file.

Can you please provide us your example reproducing the issue ? 

 

Regards

Pascal

0 件の賞賛
返信