Debugger error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugger error

6,619件の閲覧回数
ni
Contributor I
We are programing Freescale 56F8357 DSP in Metrowerks CodeWarrior IDE.
 
Our problem, derives from 2 Code Warrior IDE versions that we are using. Until now, we are working with two licenses:
 
- One fix license: CodeWarrior 56800/E Hybrid Controllers version 6.1.2
- Another floating license: CodeWarrior 56800/E Hybrid Controllers version 7.0
 
Up to now, we have debugged a program "bootloader.c" in version 6.1.2 without problems. But now, we have tried to debug using version 7.0 and we don´t arrive. Each time that we try to debug (we have Compiled and "Make" without problems), it appears a message saying "CCSProtocolPluging. CCS: Invalid Parameter".
 
We have changed our parallel port in CCS console (we have put address 0x0378) and message from CodeWarrior debugging has changed: "CCSProtocolPlugin: Unknown protocol error".
 
But after accepting this message, it appears again the message: "CCSProtocolPluging. CCS: Invalid Parameter".
 
- What could we do? What could be the solution for this problem?

We will really thank you your help with this item.
ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,796件の閲覧回数
marc_paquette
Contributor V
The cause of the problem might be conflicts with your parallel port. Is another application or service using it?
 
Alternately, this thread might help:
 
 
Let me know if the problem persists.
 
Marc.
0 件の賞賛
返信

2,796件の閲覧回数
kanu__
Contributor III

 

hi,

 

I am also facing the same error in Code warrior 3.0 for MSC 8122 ADS proeject download.

 

Here the link you provided is not working.

 

http://forums.freescale.com/freescale/board/message?board.id=CWCOMM&message.id=518 

 

 

__Kanu

0 件の賞賛
返信

2,796件の閲覧回数
J2MEJediMaster
Specialist I

Try this link instead: https://community.freescale.com/message/11176#11176. I hope this helps.

 

---Tom

0 件の賞賛
返信

2,796件の閲覧回数
kanu__
Contributor III

No. I am getting the same error again when i trying to download to 8122 board in CW 3.0.

 

The interesting thing is that , i can download into my 8101 and 8144 board using the same usb tap and code warrior versions in the same PC  now also with out any problem.

 

Earlier(2 weeks earlier) i had tested(had downloaded) the 8122 board with the same settings but i don't know what happened(no change in project) now.

 

Please help me out 

 

__Kanu

0 件の賞賛
返信