Data visualization

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Data visualization

2,602件の閲覧回数
knarf
Contributor I

Hi,

I'm using Codewarrior for DSC56800E 8.3; I'd like to monitor some variables while debugging on target board ( I use usb tap connection ). I have tried configuring "Data visualization" after launching a debug session. I can select any global variable, the graph window appears but the variable I selected is not traced on it. The same happens if I select a memory location instead of a global var. Is there any other setting that I have to configure ?

I'm also not able to pause the debug session untill the graph window is open: I have to close it and then I can pause the debug. Is that correct?

 

Many thanks

knarf

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

2,234件の閲覧回数
admin
Specialist II

As far as I understand data vizualization window refreshed while you trace application (i.e. step tracing, brakepoint tracing).

Deug window and graph window are independent - see attachment. Switch between them while debugging.

0 件の賞賛
返信