DSP56F801 flash_over_jtag and XP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DSP56F801 flash_over_jtag and XP

2,488件の閲覧回数
cwr_whitehead
Contributor I
I'm trying to use the latest version of the 'flash_over_jtag' application (Epsilon 0.7) to program two daisy chained DSP56F801's. The application ran on PC's using Window 2000. We have now upgraded to XP and the application will no longer work.
 
Whenever I try to run the application, I get the following error:
 
I/O port driver not installed
Installing...
I/O port driver cannot be started
Unable to access to I/O driver
 
Thanks in advance (hopefully).

Message Edited by CrasyCat on 2007-04-13 10:44 AM

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

696件の閲覧回数
DanielM
Contributor III
Hi,

do you have admin rights on your computer? Is it 32 or 64 bit version of XP (the program was not tested on 64-bit XP at all).

Daniel
0 件の賞賛
返信

696件の閲覧回数
cwr_whitehead
Contributor I
Hi Daniel,
 
I've solved the problem. Somehow the zlportio.sys file had been corrupted. I downloaded a new copy and replaced it, now everything works. Obvious really.
 
Thanks for the help.
0 件の賞賛
返信