DSP 56800 how to save "view array" data ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DSP 56800 how to save "view array" data ?

1,869件の閲覧回数
francospinella
Contributor I
Hi,
I'm using CW 8.0 for 56800 and USBTAP.
I need to follow the time evolution of a rapidly changing float variable (every 10 ms) , so I tried to setup a
visualization point + data visualization but I've discovered that this is extremely slow. So I've moved to
the solution of defining an array of 1000 elements, then I fill the array every 10 ms, and finally I
suspend the execution and use data -> view array to look at all the elements. This works
fine, but the problem is that I'm not able to export the content of this window to to
analyze and plot the data. ctlr +c does not work, copy is greyed ... the only solution
that I've found is to use a window capture program (snagit) that also converts to text .. but it is a
real pain. Does it exist another way to dump this data or which is the standard method of studying
the behaviour of a changing variable without slowering the system ?
thanks for your help
franco
 
 

Message Edited by CrasyCat on 2007-04-13 10:39 AM

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

619件の閲覧回数
LXC
Contributor I
I would like to know this too. Same config as the OP, except for IDE 7.3.
Options I have explored are:
-Freemaster: slow (10ms/ variable, if you have say 3 variables a variable is update at 30ms. This in spite of an update rateof 0.5ms from the target). Freemaster is also unreliable.
-tcl sripts. Arcane, difficult to figure out
-COM: see tcl
-command window , using command that are logged. Unreliable (e.g. IDE crashes if you display large amounts of memory), unable to display data memory, unable to evaluate a c pointer variable e.g. info_ptr->current
 
All I want it the content of my high speed buffer. Is this too much to ask?
What about just a little export or save as or something in the IDE?
I find this IDE very "closed", slow, unreliable and a PITA to use.
 
0 件の賞賛
返信