Concurrent Compiles

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Concurrent Compiles

1,558件の閲覧回数
ZiglioNZ
Contributor I

Hi,

 

is there any chance to enable the "Concurrent Compiles" option in CW 7.1 (coldfire) for Windows?

On the quadcore PC I use, at compile time the CPU usage doesn't go beyond 8%.

Compiling a large project takes quite a long time

Are you aware of any options that could seriously reduce the compilation time? 

 

Thanks,

Emanuel 

ラベル(1)
0 件の賞賛
返信
1 返信

1,106件の閲覧回数
CrasyCat
Specialist III

Hello

 

I do not have CodeWarrior for Coldfire V7.1 installed right now, but here is what I know from other CodeWarrior products

 

If Concurrent compilation is supported by the tool chain you should see a "Concurrent Compiles" panel in "IDE Preferences" dialog, in the General group..

 

To open IDE Preferences select entry Preferences from Edit menu.

 

If the panel is not there, concurrent compilation is snot supported.

You can submit a service request to ask for an extension.

Click here to submit a service Request.

 

CrasyCat

0 件の賞賛
返信