ColdFire PE Protocol Adapter: Stop failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ColdFire PE Protocol Adapter: Stop failed

3,764 Views
eGuy
Contributor IV

Hi,

 

I have MCF52259 evb board. My CodeWarrior version is V7.1 Build14.

 

Everyday, in the beginning, I get "ColdFire PE protocol Adapter: Stop failed" error when I try to connect to the board and debug.

 

After reset the board+reboot PC etc several times, eventually, it will work.

 

Anyone knows what the problem could be?

 

 

BTW: I also metrowerks IDE for DSP56827 and Coldfire V6.3 installed on my pc, each of them uses different type BDM/JTAG.

 

Thanks.

 

J

Message Edited by eGuy on 2009-12-04 09:58 AM
Labels (1)
0 Kudos
Reply
4 Replies

1,873 Views
J2MEJediMaster
Specialist I

Have you tried applying the 7.1.2 patch, which is available here?

 

---Tom

 

0 Kudos
Reply

1,873 Views
eGuy
Contributor IV

I have 7.1.2 Patch Build 8 installed.

 

Anyway, I will try to reinstall it ( I noticed it is 7.1.2a from the link you give) and see the result.

 

Thanks.

 

J

0 Kudos
Reply

1,873 Views
Salvatore
Contributor I
0 Kudos
Reply

1,873 Views
Salvatore
Contributor I

Hi,

I'm using the MCF5485RM, and I'm working on target.

I've ColdFire 7.1 and installed the patch 7.1.2, but when I want work in debug mode, on the PC is present the popup

ColdFire PE Protocol Adapter: Stop failed.

 

0 Kudos
Reply