Codewarrior version 3.2.1 macro _CW_X_SLLD_ related problem + for 64bit divsion

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior version 3.2.1 macro _CW_X_SLLD_ related problem + for 64bit divsion

1,983件の閲覧回数
puru
Contributor I
Hi ,

Currently i m using codevarrior version 3.2.1. In which i m using 64 bit operation for that i placed -slld option in passthrough (To shell ) section of project setting .

but by doing so i m facing problem in sqrt function .

because CW_X_SLL macro is not enable in rtlib library c file .
but if i will include those file in my project then this macro will be enabled.

It is not possible to include all rtlib files in my project, can any body suggest how can I overcome such problem?
ラベル(1)
0 件の賞賛
返信
1 返信

920件の閲覧回数
CrasyCat
Specialist III
Hello
 
In order to enable operation on 64-bit data, can you please check the box "64-Bit Data Type support (long long and double)" in the "C Language" panel.
This should change the library linked to your application and enable the appropriate sqrt function.
You should also remove th e-slld option from the passthrough section of project settings.
 
If this s not help can you check in the .map file generated by the linker which is the run time library linked to your project.
 
CrasyCat
0 件の賞賛
返信