Codewarrior is conflict with the newest Nvidia graphic driver!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior is conflict with the newest Nvidia graphic driver!

1,532 Views
onemoretouch
Contributor I

I am using a Dell notebook whose graphic card is Nvidia's Quadro NVS 160M. Before I just installed the driver with the version of 179.68. There were no problem with codewarrior. Everything goes well.

 

Lately Nvidia update the driver to 189 or 19* series. The new driver is much more compatible with windows 7 and gives more powerful performance. But after installed the new driver, codewarrior meets some problem: the software can be opened normally, but when I load a project or open a file, codewarrior is crashed! It says that IDE.exe meet some problem. I have installed codewarrior 6.3 for coldfire V1 and 5.0 for S12X, both editions have the same problem. It seems that the problem comes out from this file "IDE_MFC60cw.dll". Is this a overload dll of MFC60.dll? What is wrong with it?

Labels (1)
0 Kudos
Reply
2 Replies

863 Views
J2MEJediMaster
Specialist I

The problem you describe sounds similar to one that occurred some time ago when certain software was installed with Microsoft Office. (The IDE crashed when you try to use a standard file dialog). I would suggest looking at the following FAQ and see if the work-around can help here:

 

FAQ-27815

 

Hope this helps.

 

---Tom

Message Edited by J2MEJediMaster on 2010-01-20 08:35 AM
Message Edited by J2MEJediMaster on 2010-01-20 08:36 AM
0 Kudos
Reply

863 Views
onemoretouch
Contributor I

Thank you very much!

According to the FAQ, the only way to solve the problem is to remove the newest Nvidia graphic driver. Hope Codewarrior could find what's wrong with itself!

0 Kudos
Reply