Codewarrior for DSC - how do I assign a constant to be at a specific address in code ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Codewarrior for DSC - how do I assign a constant to be at a specific address in code ?

2,043 次查看
Radar99
Contributor I
How can I assign a constant to be at a specific address in code. I want the const variable "CAL_DATA" to be at the address F000 ? In Codewarrior for Microcontrollers  I used the following:
 
const word CAL_DATA @0xF000 = 0x1234;
 
However, this does not work for Codewarior for DSC compiler.
 
Thanks
 
标签 (1)
标记 (1)
0 项奖励
回复
1 回复

712 次查看
Visitor08
NXP Employee
NXP Employee
Only limited support exists for non-constant data.
 The constant value specified after ":" is the word address of the global variable, i.e. for 
    int OneReg : 0xBCD ;
  the global variable OneReg resides at word address 0xBCD
  NOTE: the linker does not reserve space for global variables declared with ":" operator
0 项奖励
回复