Codewarrior for 56364?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior for 56364?

2,797 Views
FredrikW
Contributor I
Where can I find codewarrior for DSP56364?
Is it same as for Starcore?
Can I use Symphony Studios instead of codewarrior?
What do you recommend?
 
Fredrik
Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,288 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
CodeWarrior doesn't support the 56364.
Please refer to the link below for details:
 
Regards
Pascal
0 Kudos
Reply

1,288 Views
J2MEJediMaster
Specialist I
No, that isn't a StarCore part. StarCore DSP part numbers start with either MSC or SC. See this page. Go to the CodeWarrior for DSP page on this web site and see if it supports this part. I've not heard anything about Symphony Studios and so I can't comment on it.

---Tom
0 Kudos
Reply