Codewarrior for 56364?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior for 56364?

2,787件の閲覧回数
FredrikW
Contributor I
Where can I find codewarrior for DSP56364?
Is it same as for Starcore?
Can I use Symphony Studios instead of codewarrior?
What do you recommend?
 
Fredrik
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,278件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
CodeWarrior doesn't support the 56364.
Please refer to the link below for details:
 
Regards
Pascal
0 件の賞賛
返信

1,278件の閲覧回数
J2MEJediMaster
Specialist I
No, that isn't a StarCore part. StarCore DSP part numbers start with either MSC or SC. See this page. Go to the CodeWarrior for DSP page on this web site and see if it supports this part. I've not heard anything about Symphony Studios and so I can't comment on it.

---Tom
0 件の賞賛
返信