Codewarrior file system question.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior file system question.

ソリューションへジャンプ
3,424件の閲覧回数
schmighty
Contributor I

I want to maintain a working backup of my project's source files to fall back upon when I make a bold revision in code. How do I save those backup files in codewarrior? It seems that just copying the project directory and working out of those files/directories results in changes that are reflected back to the original files/directories I copied them from. I was fooled in the thought (for years now) that just making a copy of the project directory would leave me with a "saved and working" original project folder, but codewarrior changes those supposily "saved and working" original source files too. What's the fix?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,829件の閲覧回数
J2MEJediMaster
Specialist I

1) Make a duplicate of the CodeWarrior project directory.

2) Open the project file (.mcp) in the duplicate directory.

3) Go to the project's settings panel. (Type ALT-F7.) Next, go to the Access Paths panel and ensure that there are no hard-coded directory paths in there. (For example,  C:\DSP_Filters\FIR\sources.) There should only be project-relative paths present (for example, {Project}sources).

4) Choose Project > Reset Project Entry Paths

5) Choose Project > Re-search for Files.

 

That should clear out any directory info of the previous project.

 

---Tom

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,829件の閲覧回数
schmighty
Contributor I
Thank you, that took care of my problem.
0 件の賞賛
返信
1,830件の閲覧回数
J2MEJediMaster
Specialist I

1) Make a duplicate of the CodeWarrior project directory.

2) Open the project file (.mcp) in the duplicate directory.

3) Go to the project's settings panel. (Type ALT-F7.) Next, go to the Access Paths panel and ensure that there are no hard-coded directory paths in there. (For example,  C:\DSP_Filters\FIR\sources.) There should only be project-relative paths present (for example, {Project}sources).

4) Choose Project > Reset Project Entry Paths

5) Choose Project > Re-search for Files.

 

That should clear out any directory info of the previous project.

 

---Tom

 

 

0 件の賞賛
返信