Codewarrior Install on Windows 7 64bit - mac_mot.sys error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior Install on Windows 7 64bit - mac_mot.sys error

4,001 Views
bchriste
Contributor I

I have been running codewarrior 5.2.1177 on my XP machine for years.  I have a new Windows 7 64bit machine that I need to test with.  I have installed / uninstalled / reinstalled codewarrior as administrator and rebooted the comptuer many times.  I have gone throught the documentation and run the mac_mot.sys and mac_mot.ini files.  The mac_mot.sys file is in the windows/system32/drivers folder and I have checked the register to verify it is in the correct place.  I can get it to compile but each time I try to run the parallel port to start debugging i get the message box "NT DRIVER NOT FOUND: MAC_MOT.SYS".

 

Any ideas

 

Thanks

Bruce

Labels (1)
0 Kudos
Reply
2 Replies

2,066 Views
felixk
Contributor I

To all that this may concern,

 

To rectify the mac_mot.sys error please visit http://macraigor.com/FAQ.htm#mac_mot and read their instructions. You may need to reinstall Codewarrior if this error resulted after the installation of a Codewarrior product. Ensure mac_mot.sys in is in your system folder e.g. C;\Windows\system32

 

Regards,

 

felixk

0 Kudos
Reply

2,066 Views
J2MEJediMaster
Specialist I

Based on the error message mentioning the lack of a driver, I would hazard a guess that a parallel port driver is missing.

 

---Tom

0 Kudos
Reply