Codewarrior Eclipse on Linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Codewarrior Eclipse on Linux

13,105 次查看
juanpgaviria
Contributor I

I've been testing the Codewarrior Eclipse on linux. 

Is there any specific place to get info and/or help on this subject?

标签 (1)
0 项奖励
回复
22 回复数

9,102 次查看
Ari
Contributor I

Hi. I've just installed CW Beta 10 on a Linux PC (Athlon x2 - 4 Gb RAM - Ubuntu 9.10 64bits) and i wanted to test it.

I'm NOT experienced at all with eclipse, and don't have much practice on CW either, but i've made a couple of simple programs for HCS08 MCUs. 

 

My problem with CW Beta 10 is the Processor Expert. I use the Device Initialization, wich is (i believe) a part of Processor Expert, but when i tried to create my 1st proyect on Beta10, i get a prompt message saying something about a "local sever" for Processor Expert, and that that can only be used on a Windows PC.

 

If anyone can help me with this, i'd be mostly thankfull. I don't know if this is a particular problem on my computer, or if it's a general problem with Linux and Beta 10.

 

Thanks!! 

 

Ari

 

P.S.: I've build an OSBDM with a JB16 (20 pin version). It worked OK on CW 6.3 under Windows. Does it also work on Beta 10 in Linux? I couldn't try it because of the upper issue.

0 项奖励
回复

9,102 次查看
xtronics
Contributor I

I got it to put up a window - but it would not let me pick the chip I'm using - put up errors. I wish I could find  a serious support area - should be an eclipse-on-linux forum area or at least a page describing what is available and a time line.  Was there a previous version that supported HCS08 development on Linux?  A link please?   

0 项奖励
回复

9,102 次查看
J2MEJediMaster
Specialist I

There are links to support on the CodeWarrior for MCUs v10 beta page.

0 项奖励
回复

9,102 次查看
xtronics
Contributor I

 


J2MEJediMaster wrote:

There are links to support on the CodeWarrior for MCUs v10 beta page.


OK?  How about a hint - I look at your link and I see videos - I look at the download tab - just the package? I'm just not seeing this download - exactly what is the file name and how do I get to it?
I need to work with the HCS08...  I have MCU_10_Linux installed and running .. (should I just ignore the license complaints?
So others know - there is no eclipse executable as mentioned in the documentation (a launch script by that name might be nice) - there is a /eclipse/startup.jar that you need to run with Sun-Java5-Runtime(32bit) which requires you install ia32-sun-java5-bin on Debian and all of the Debian descendants OS's - Debian lenny has all the required libs according to the install.
On start up it complains about a License -
Cannot load flexlm license from :${MCU_TOOLS_HOME}/license.dat 
Yet when I look in MCU_10.0 there is a license.dat file??
Clicking on details:
Detail information for product "MCU" version "1.0.0"
status: "Cannot load flexlm license from : ${MCU_TOOLS_HOME}/license.dat"
License model: "class com.freescale.core.ide.license.flexlm.FlexlmActivate"
Contact Email: [email protected]
Register URL: http://www.freescale.com/webapp/sps/site/homepage.jsp?nodeId=02Wcbf
Purchase URL: http://www.freescale.com/
FlexLM Eval Period: 15 day(s)
GTL Server: gtlsrvr.metrowerks.com
GTL Port: 80 (8,080)
Wants Host ID: true
License file path:
flexlmFileLocator: null
flexlmFile: ${MCU_TOOLS_HOME}/license.dat
License file URL: null
Error String: Cannot load flexlm license from : ${MCU_TOOLS_HOME}/license.dat
Feature Keys:
FEATURE ProfessionalEditionMCU 10.0, status : INITIALIZATION_ERROR
Alternate Keys:
(no keys)
LM_PATH=null
License file Content:
 (License file not found)

Ignoring the license issue seems to work?  
The file bar seems to have either a break or is missing some menu between RUN and PROCESSOR Expert
Clicking on Processor Expert/component wizard complains:
The chosen operation is not currently available.




 

 

0 项奖励
回复

9,102 次查看
ProcessorExpert
Senior Contributor III

Hello,
 
regarding to question about PE and CW 10.0 and Linux - please note that some parts of Processor Expert still needed to be run in Windows enviroment even you have CW 10.0 beta on Linux, hence is there the message about using PE on Windows PC.
 
I think it is a general problem in beta 10 and it will persist in CW 10. FINAL. To avoid the problem it is recommended to start PE server onto another PC with Windows.
 
In case that you have not another PC there is possibility to use "Wine" to workaround the problem. However it is not supported solution and it was only tested within 32-bit Debian distribution.
 
For more details about using Wine on 64-bit platform please follow this link: http://wiki.winehq.org/WineOn64bit
 
Helper script tested on Debian to configure clean install of  Wine for using with Processor Expert:
 
#!/bin/sh
# tested with wine version wine-1.0.1
wget http://www.kegel.com/wine/winetricks
# sudo apt-get install cabextract
./winetricks msxml3 msxml6 winxp

Ports used for communication are 9998 and 9999.

 

best regards
Vojtech Filip
Processor Expert Support Team

0 项奖励
回复

9,102 次查看
Ari
Contributor I

Hi, I don't mean to be rude, but I don't understand why is there a Linux version of CW if it cannot be used without a windows platform, and, as I understood from an answer above, it won't be fixed in the final version? I though that the Processor Expert (and Device Initialization) problem on Linux would be fixed eventually, and that it would be released on a final version, but if it's not going to be that way, why bother on releasing a Linux version of CW that cannot be fully used on Linux as a standalone development suite?

 

Again, I'm sorry if I offended anyone, but I just don't see the point. Maybe there is a purpose on this release that I, as I'm still in college, don't know of, but I think the CW 10 should be used on Linux as on a Windows PC, without the need of a windows server. 

0 项奖励
回复

9,102 次查看
CompilerGuru
NXP Employee
NXP Employee

First, I really don't know anything about the PE integration in Linux.

But even without PE, CW can be used to as a "as a standalone development suite".

Writing code, building it and using source code debugging is supported natively. That there is one RAD feature not supported without having something running on a windows server is unfortunate, but it does not make the rest unusable.

 

Daniel

0 项奖励
回复

9,102 次查看
Sanahuja
Contributor I

Hi,

 

I'm having the same problem with device initilization under Linux. I have done:

./winetricks msxml3 msxml6 winxp

but I don't understand what I have to do next....

Could you be more precise about how to settup the  PE server using wine?

 

Thanks.

Regards,

Guillaume Sanahuja.

0 项奖励
回复

9,102 次查看
xtronics
Contributor I
Pay attention to the output of ./winetricks msxml3 msxml6 winxp I got a bunch or error - seems like it is for an older version of wine? What version of winetricks did they use? - it has a new date code 24-Apr-2010 - so we may not be looking at the same thing. At the very least tell us the version numbers of wine on the working system so we can debug this. By calling this software 'beta' you have raised expectations that are not realistic. Linux folks can get this to work under wine if we have the details of the configuration. It appears that we need to install some programs from Microsoft - via winetricks. If you can make this work on a Debian box - most any Linux system will then work (Most distributions directly or indirectly pull their packages from there.) A ETA of when a Linux beta of PE is coming would be nice. It would take someone with a working system about an hour to write up the versions and steps to set this up under wine. Linux folks don't need lots of hand-holding, but a few breadcrumbs would be appropriate.
0 项奖励
回复

9,102 次查看
xtronics
Contributor I
I got PE to run under wine -- but eclipse processor_expert/component_wizard still says: "The chosen operation is not currently available. " If someone that has this running could provide copies of the exact command line, versions etc. The 'instructions' spoke of tow port numbers - there seems to be only one command switch to set a single number?
0 项奖励
回复

9,102 次查看
ProcessorExpert
Senior Contributor III

 

Hello,

 

- Regarding to the question on running Component Wizard under Linux platform: Unfortunatelly Component Wizard is not suported under Linux because its currently still windows app. only. However, you can try to run the windows execuable, but there will be probably issues with transfering components to PE.
 
- Here are summarized instructions of runnig PE in wine:

 

#!/bin/sh
sudo apt-get install wine
# tested with wine version wine-1.0.1
wget http://www.kegel.com/wine/winetricks
# sudo apt-get install cabextract
./winetricks msxml3 msxml6 winxp
 
Then it's necessary to have PEsrv.exe, which unfortunatelly is not a part of Linux beta version. So you need to:

- Get also the windows version, install it somewhere and then take PEsrv.exe from it's layout ({instal dir}/MCU /ProcessorExpert/PEsrv.exe and place it to the same directory onto your linux version.

 - Then start the Eclipse, Select Window / Preferences and choose Processor Expert / Processor Expert Server. Then select User remove server and set the removte server settings to address 127.0.0.1 and port 9999.

- The close CodeWarrior and start PEsrv.exe calling the following command in the {instal dir}/MCU/ProcessorExpert directory: wine PEsrv.exe

- Then start CodeWarrior and Processor Expert should be working.

best regards
Vojtech Filip
Processor Expert Support Team
0 项奖励
回复

9,102 次查看
xtronics
Contributor I

Processor Expert / Processor Expert Server

 

No such option appears in the Processor Expert menu - I've verified that PEsrv.exe is running.

 

Does PEsrv.exe need to be started with any command-line switches?

 

PEeclipseSrv.exe [-port portnumber][-shutdown][-help]

 -port       Specify Processor Expert server port <portnumber>
 -server     Start Processor Expert server
 -shutdown   Stop Processor Expert server, disconnect all active connections
 -log        Create log in /Logs directory
 -help       Show this help


0 项奖励
回复

9,102 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

It is not in Processor Expert menu. As I wrote in my previous post you should use the menu command Window -> Preferences.

See the attached screenshot.

 

No command line switches are necessary for PEsrv.exe. 

 

best regards
Vojtech Filip
Processor Expert Support Team

0 项奖励
回复

9,102 次查看
xtronics
Contributor I

"Then select User remove server and set the removte server settings to address 127.0.0.1 and port 9999."

 

From above should read "Then select User remote server and set the remote server settings to address 127.0.0.1 and port 9999.

 

 

Also - this will not work with Java 5 runtime (32 bit) (throws up an error: Unable to create the selected preference page.
Bad version number in .class file) - only Java 6.

 

And now doing new bareboard project returns an empty list of devices - see attached.

 

.. confirmed PE is running:

 

$wine-auto PEsrv.exe
fixme:console:AttachConsole stub ffffffff

Processor Expert server application
(C) Freescale Semiconductor, Inc. All Rights Reserved.

Server is already running


 

 

 

 

 

0 项奖励
回复

9,102 次查看
xtronics
Contributor I
I'm back on this with a newer version. I'm now dealing with: "The P&E USB driver did not install properly." It appears that I need to be able to reconfigure to build it for x86_64 configure: error: You are trying to install WinDriver for i386 on x86_64. configure: error: You are trying to install WinDriver for i386 on x86_64. make[1]: makefile.usb.kbuild: No such file or directory make[1]: *** No rule to make target `makefile.usb.kbuild'. Stop. make: *** [clean] Error 2 make[1]: makefile.usb.kbuild: No such file or directory make[1]: *** No rule to make target `makefile.usb.kbuild'. Stop. make: *** [all] Error 2 make[1]: makefile.usb.kbuild: No such file or directory make[1]: *** No rule to make target `makefile.usb.kbuild'. Stop. make: *** [all] Error 2 From http://www.jungo.com/st/support/installation_instructions.html#install_linux Installation Instructions for Linux System Requirements * Any 32-bit x86 processor with a Linux 2.2.x (PCI/ISA only), 2.4.x or 2.6.x kernel or: Any 64-bit x86 AMD64 or Intel EM64T (x86_64) processor with a Linux 2.4.x or 2.6.x kernel
0 项奖励
回复

9,102 次查看
xtronics
Contributor I

I'm back on this with a newer version.  I'm now dealing with:

 "The P&E USB driver did not install properly."

It appears that I need to be able to reconfigure to build it for x86_64

configure: error: You are trying to install WinDriver for i386 on x86_64.
configure: error: You are trying to install WinDriver for i386 on x86_64.
make[1]: makefile.usb.kbuild: No such file or directory
make[1]: *** No rule to make target `makefile.usb.kbuild'.  Stop.
make: *** [clean] Error 2
make[1]: makefile.usb.kbuild: No such file or directory
make[1]: *** No rule to make target `makefile.usb.kbuild'.  Stop.
make: *** [all] Error 2
make[1]: makefile.usb.kbuild: No such file or directory
make[1]: *** No rule to make target `makefile.usb.kbuild'.  Stop.
make: *** [all] Error 2



From http://www.jungo.com/st/support/installation_instructions.html#install_linux

Installation Instructions for Linux

System Requirements

    * Any 32-bit x86 processor with a Linux 2.2.x (PCI/ISA only), 2.4.x or 2.6.x kernel
      or:
      Any 64-bit x86 AMD64 or Intel EM64T (x86_64) processor with a Linux 2.4.x or 2.6.x kernel

0 项奖励
回复

9,102 次查看
xtronics
Contributor I

Now working with a i386 box

 

Looks like something isn't specified:


Cannot get env. variable ALLUSERSPROFILE

 

Then later:


java.lang.UnsatisfiedLinkError: Can't load library: /home/karl/workspace/../../ide/Output/IDEDebug/libCWNative.so

 

Looks like a bad path to me.

 

I've attached the whole mess.

 

0 项奖励
回复

9,102 次查看
xtronics
Contributor I

It appears that PEsrv.exe service running on a windows box  is needed for device initialization to run on Linux - can someone verify that for me?

 

Is "device initialization" provided by the processor expert server?

 

 

0 项奖励
回复

9,102 次查看
xtronics
Contributor I

The available update for 10.0  from http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=012726006178829C6F9CBE fails

 

 

I've attached the log file - - tried installin gupdates in different orders etc..

 

If you do this - you can get back to square one by deleting your ~/.eclipse directory

0 项奖励
回复

9,102 次查看
xtronics
Contributor I

ProcessorExpert wrote:


...regarding to question about PE and CW 10.0 and Linux - please note that some parts of Processor Expert still needed to be run in Windows enviroment even you have CW 10.0 beta on Linux, ...


 

Ok - how about a link to the windoze version of PE we would need to run?

With a file name?

 

(Are you sure you want to call this "beta" at this point? ) 

 

 

0 项奖励
回复