Codewarrior 10 Beta [Win] & MQX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior 10 Beta [Win] & MQX

1,903件の閲覧回数
JMiguez
Contributor I
Currently evaluation of CodeWarrior 10 Beta (with Eclipse) is being evaluated at the office by engineers.
There are a set of issues of importance to be addressed as quick as possible to make the next version of the software as rugged as possible. These issues are as follows:
1. The USB port fails at install time.
2. MQX is not compatible with the program, therefore it is rather impossible to use RTOS and other excellent communication tools.
This is a critical update that should be included in, see attached picture "Incompatibility_MQX.jpg".
3. The program needs to be a little bit more intuitive, a better user-friendly program to attract more programmers.
4. Keywords inside comments produce warning (and possibly errors too). See attached picture "CommentWarning.jpg".
5. More videos are encouraged!
ラベル(1)
0 件の賞賛
返信
1 返信

1,014件の閲覧回数
J2MEJediMaster
Specialist I

1) File a Service Request on this. Click here to do that.

2) Have you tried, per the error message, to do a manual install? If that did not work. or the documentation references the old "Classic" CodeWarrior directory layout, then file a service request on that.

3) Various settings and controls are found in different locations in Eclipse IDE versus the old Classic CodeWarrior IDE. It takes some getting used to, and I agree that certain things (such as the build settings) are buried several levels deep when compared to the Classic UI. The engineers are adding extensions to faciltate certain actions, but some of it just simply the way the Eclipse UI is laid out.

4) File a SR on that. See 1).

 

Please note that Help is available by pressing F1 or clicking the question mark icon. The manuals are all in electronic format and can be searched from within the Eclipse IDE. For certain operations (such as in the New Project wizard or the Debugger tabs in the Launch Configurations dialog), a help request will bring up the relevant page of the Targeting manual that explains the various setttings on that page of the wizard.

 

0 件の賞賛
返信