Codewarrior 10.1 with win7 64bit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior 10.1 with win7 64bit

ソリューションへジャンプ
4,597件の閲覧回数
terra
Contributor I

Just down load and install CW 10.1 on Win7X64bit machine. I use the example project for HCS08 then import the projet then press re build all at it shows me error on main_asm on line 0

 

What could be the probelm?

ラベル(1)
0 件の賞賛
返信
1 解決策
3,340件の閲覧回数
CrasyCat
Specialist III

Hello

 

It looks like the problem is related to the installation path.

Can you please Try to uninstall CodeWarrior and re-install it in a path without any space in the fullpath.

        For instance c:\Freescale

 

Is it working better?

 

If this is the case,  I would recommend you to submit a service request for that.

Spaces should be accepted in path names.

Click here to submit a service request.

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
3,340件の閲覧回数
CrasyCat
Specialist III

Hello

 

Which sample project are you using?

 

What is the message you are getting (Whole message please)?

 

CrasyCat

0 件の賞賛
返信
3,340件の閲覧回数
bla5029
Contributor I

Make sure win windows 7 you are running Codewarrior as administrator.

 

I have been working with the webserver demo I am also getting that error.  I notice that it will not give me normal errors for syntax mistakes.  This is the only error i have recieved.  Is there something configured wrong in my project?

0 件の賞賛
返信
3,340件の閲覧回数
terra
Contributor I

I try most of the example and giving me the same error

here is soem screen shots

0 件の賞賛
返信
3,340件の閲覧回数
CrasyCat
Specialist III

Hello

 

  1- Can you please copy content of the Console window and send it over?

      Console will contain more details than Problem view.

 

  2- If you are programming in assembler, directives and instructions cannot start on column 1.

      Please insert at least 1 space or TAB in front of the XDEF and include instruction.

 

CrasyCat

0 件の賞賛
返信
3,340件の閲覧回数
terra
Contributor I

1. Here is the attachement

2. Thanks for the info

0 件の賞賛
返信
3,341件の閲覧回数
CrasyCat
Specialist III

Hello

 

It looks like the problem is related to the installation path.

Can you please Try to uninstall CodeWarrior and re-install it in a path without any space in the fullpath.

        For instance c:\Freescale

 

Is it working better?

 

If this is the case,  I would recommend you to submit a service request for that.

Spaces should be accepted in path names.

Click here to submit a service request.

CrasyCat

0 件の賞賛
返信
3,340件の閲覧回数
terra
Contributor I

Thanks mate, it is working fine with C:\FreeScale

0 件の賞賛
返信
3,340件の閲覧回数
bla5029
Contributor I

had that problem with 10.0, and changing the direction path for the project seems to work as well.  The MQX was looking in program files, not program files x86, just throw the x86 in on the path and it picks up and runs with it.

0 件の賞賛
返信