Codewarrior 10.1 problem by installing new software..

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior 10.1 problem by installing new software..

2,855件の閲覧回数
monXii
Contributor III

Hello,

i installed the Codewarior 10.1 on my Windows 7 64 Bit System.

No problem .. But then i installed all the new Software from this URL (http://freescale.com/lgfiles/updates/Eclipse/MCU10_1/com.freescale.mcu.updatesite/) via Eclipse > Help > Install new software ..

 

And after a while this error occures =/

 

An error occurred while installing the items
  session context was:smileysad:profile=PlatformProfile, phase=org.eclipse.equinox.internal.provisional.p2.engine.phases.Install, operand=null --> [R]com.freescale.mcu10_1.beekit.win.sp_root 1.0.1, action=org.eclipse.equinox.internal.p2.touchpoint.natives.actions.RemoveAction).
  Directory is not empty: C:\Program Files (x86)\Freescale\CW MCU v10.1\eclipse\..\MCU\ARM_EABI_Support\Memory_Config_Files
  Directory is not empty: C:\Program Files (x86)\Freescale\CW MCU v10.1\eclipse\..\MCU\ARM_EABI_Support\Memory_Config_Files

 

when i remove this folder, it has some error by another folder ..

 

what's the problem? whats wrong? where is my fault? :smileyhappy:

 

i need the updates cause i want to use MQX 3.7 on K60 ..

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,433件の閲覧回数
monXii
Contributor III

Hello again..

 

i installed CW10.1 on my Win Xp 32 Bit Notebook..

 

All is fine!

 

Someone else problems with Win 7 64 Bit?

Or is there someone who runs CW10.1 with all updates on Win 7 64 Bit? =)

0 件の賞賛
返信

2,433件の閲覧回数
edwardjpalmer
Contributor I

I get the same error.  Tried everything short of uninstalling the entire CodeWarrior suite and starting fresh.  I am also running Win7 64-bit.

 

All software updates worked except for two:

CodeWarrior Core IDE, v1.0.1

CW MCU v10.1 Update, v1.0.1

 

I then ran the CodeWarrior executable in Windows XP SP3 compatibility mode.  All the updates appeared to work just fine!

0 件の賞賛
返信

2,433件の閲覧回数
CrasyCat
Specialist III

Hello

 

Did you try installing CodeWarrior outside of the  C:\Program Files (x86) directory?

 

Try using C:\Freescale as root installation directory instead of C:\Program Files (x86)\Freescale.

Also make sure you are logged in with Administrator right to do the install.

 

CrasyCat

0 件の賞賛
返信

2,433件の閲覧回数
sps
Contributor I

I have the same error during CW10.1 update installs. Without the updates, not possible to build the MQX libs. I don't want to change paths all over the place since this complicates moving projects across platforms.

 

Any solutions yet, other than installing from root (not a great solution) - not looking forward to one more uninstall/reinstall dance with CW & MQX.

 

System: Dell Optiplex I7, Win7 Pro x64.

 

Thanks - Steve

 

0 件の賞賛
返信

2,433件の閲覧回数
CrasyCat
Specialist III

Hello

 

There is an Update Procedure document that explains how to install the Compiler Update (http://www.freescale.com/files/soft_dev_tools/doc/support_info/CW_MCU_v10.1_Update_Procedure.pdf) in offline or online mode. 

 

Try using off-line mode.

 

CrasyCat

0 件の賞賛
返信