CodeWarrior sample code for 56F8367

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior sample code for 56F8367

2,758 次查看
maria_m
Contributor I
I currently have a project to create a FW for 56F8367 Microprocessor. I have no experience with embedded design, I am totally new in this field. However I manage to play around CodeWarrior.


I want to know if anyone can share a sample code in creating a FW.The schematic diagram of my project would need to access the following: PWM, CAN, JTAG, ADC, GPIO, LED, FSRAM and others. I was able to configure JTAG using USB Tap and to make LED work.


If anyone can provide a pattern/ sample source code that I can easily study, i would really appreciate. I only have limited time for this project.


I hope someone can help out. Big thanks in advance.
标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,270 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

 

I don'thave this example but the installation contains lot of examples.

Processor Expert is a rapid application design tool integrated into CodeWarrior tool suites for the HC(S)08/RS08, HCS12(X), DSC and ColdFire architectures. It combines easy-to-use component-based application creation with an expert knowledge system.

This application will help you to create your application.

 

You will find some example based of Processor Expert on your installation:

 \Stationery\Processor_Expert_Examples

 

I don't know the tool version used.

The last version is CodeWarrior Development Studio for Freescale 56800/E Digital Signal Controllers Version 8.2.3

You can download this version on our web site via the link:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC

For details please have a look in:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC&tab=In-Depth_Tab

In the download tab you can download the Special Edition or the Evaluation.

The Special edition contains the special edition license limited to 32 kb of Code.

We recommend you to download the Evaluation edition.

A Professional Evaluation license is provided for first 30 days.

After 30 days the product will function at the Special Edition level.

 

Hope this will help you.

Pascal

0 项奖励
回复