CodeWarrior for Palm OS - 9.2 update causes crashing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior for Palm OS - 9.2 update causes crashing

2,245件の閲覧回数
Griffariff
Contributor I
I installed CodeWarrior 9 for Palm OS on my newly rebuild Win XP computer (no additional SDK elements or updates were installed). I installed the 9.1 update and rebuilt the BuildAll.mcp project successfully. When I went to modify access paths for a project, it worked. I installed the 9.2 update and rebuilt the BuildAll.mcp as per the instructions. When I went to check/modify the access paths for the BuildAll project it crashes/closes CodeWarrior. Am I doing something wrong here?
 
I tried installing the 9.3 update to see if it would correct this issue and it does not. Everytime I click on the Add button to add and access path, CodeWarrior crashes. This is a sparkling clean, newly reinstalled Win XP installation. It was behaving this way before the rebuild as well. HELP!!!
ラベル(1)
0 件の賞賛
返信
1 返信

1,102件の閲覧回数
CrasyCat
Specialist III
Hello
 
This product is not supported by Freescale. You may email [email protected] with your question about these unsupported product.
 
You may also find assistance on a Palm programming forum.
 
I hope this helps.
 
CrasyCat
0 件の賞賛
返信